2025-10-27 5:12 AM - edited 2025-10-27 5:22 AM
I am working with STM32H747I -DISCO board
I am using CubeMx version 6.15, firmware: H7_V1.12.2, Freertos CMSIS2 - V10.3.1
configuration 1 : Generating from touchgfx and configuring Eth other all parameters commented in code (Touchgfx parameters).
Here ETH is working fine
configuration 2 : only configuring ETH with same configurating as above but generating from cubemx
Here Eth Communication worked for abt 10 to 20 min and then MCU stucked.
I compared both projects : it's all same (MPU configuration Linker script DMA Descriptor and RAM Heap pointer) ...middleware package, CMSIS files, Freertos config files, Lwip folder(lwip.c .h and ethernetif.c and lwipopt.h),LAN files all are same but still I am facing this issue.
I have attached wireshark snip when MCU got stucked
and IOC files 1. Touchgfx generated 2. CubeMx Generated
Solved! Go to Solution.
2025-10-28 2:53 AM - edited 2025-10-29 2:53 AM
Set the TCPIP priority higher
increase MCU STACK and HEAP
Changed CMSIS v2 to V1
2025-10-27 6:08 AM
A program failing after 10-20 minutes could mean an issue with memory handling. Perhaps you are leaking memory, or a buffer write it out of bounds. Pause the program when it's "not working" and figure out the symptoms and cause.
2025-10-28 2:53 AM - edited 2025-10-29 2:53 AM
Set the TCPIP priority higher
increase MCU STACK and HEAP
Changed CMSIS v2 to V1
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.