2026-03-03 1:59 PM
Hello everyone,
I've been working on getting Ethernet working on the STM32H750B-DK discovery board with TouchGFX and LwIP. After extensive debugging, I suspect a hardware issue and would appreciate your advice on confirming this.
TouchGFX display runs perfectly
USART3 debug output works (Tera Term shows messages)
PHY communication works (we get "Link established!")
The Ethernet MAC peripheral itself appears completely dead. We've tried:
Successfully read PHY registers
PHY responds and reports link up
This proves MDIO/MDC pins are working
ETH DMACSR after reset: 0x00000000
ETH DMACSR after system reset: 0x00000000Reading ETH->DMACSR always returns 0
This register should never be 0 on a live peripheral
Software attempts:
Enabled all ETH clocks (__HAL_RCC_ETH1MAC_CLK_ENABLE() etc.)
Forced and released peripheral reset
Tried system-level reset via RCC (RCC_AHB1RSTR_ETH1MACRST)
De-init and re-init with correct descriptors (0x30040000 etc.)
Bypassed MX_LWIP_Init() completely
Manual PHY configuration (gets link)
CubeMX configuration verified:
ETH set to RMII mode
All RMII pins correctly assigned (PA1, PA2, PA7, PC1, PC4, PC5, PG11, PG13, PG14)
LAN8742 PHY selected
Linker script has proper .lwip_sec section at 0x30040000
ETH DMACSR after reset: 0x00000000
ETH still not responding - trying system reset
ETH DMACSR after system reset: 0x00000000
ETH HAL Init FAILED with error: 1The DMACSR register should never read 0 on a working peripheral. Even with no link, it should return a non-zero value.
Is DMACSR = 0 definitive proof of dead hardware? What else could cause this?
Are there any jumpers or solder bridges on the STM32H750B-DK that need to be closed for Ethernet to work?
What should DMACSR read on a properly functioning STM32H750? (Even with no cable?)
Any way to verify if the ETH peripheral is getting power/clocks?
Could this be a faulty chip/board? The board is new and the display works perfectly.
Is there a factory demo that uses Ethernet I can flash to confirm hardware works?
Pre-RTOS: UART is working!
About to start RTOS...
LWIP task STARTING...
Manually configuring PHY...
Link established!
ETH power-up sequence...
All ETH clocks enabled
ETH reset released
ETH DMACSR after reset: 0x00000000
ETH still not responding - trying system reset
ETH DMACSR after system reset: 0x00000000
RxDesc: 0x30040000, TxDesc: 0x30040100, RxBuffLen: 1536
ETH HAL Init FAILED with error: 1
Setting up network interface...
IP set to: 192.168.1.110
Network interface is UP
Starting echo servers...
Heartbeat #0 - IP: 192.168.1.110Any help would be greatly appreciated! I've spent days on this and suspect hardware failure, but want to be certain before replacing the board.
Board: STM32H750B-DK DK32H760B$AT1
CubeMX Version: 6.16.0
TouchGFX Version: 4.26.0
Ethernet PHY: LAN8742 (onboard)
Thanks in advance!
Solved! Go to Solution.
2026-03-04 8:58 AM
If you have generated a project from scratch in CubeMX, it isn't guaranteed to work. Start from some ready example from the Projects subdir in the Cube package, or from here.
2026-03-03 3:05 PM - edited 2026-03-03 3:08 PM
What example project do you use for the ETH & LwIP? Is this one of ST provided examples or something else?
2026-03-03 10:54 PM
2026-03-03 11:30 PM
I'm working with ETH on H723 .. H735 - I'm not 100% sure if ETH is the same as in H750.
Why should DMACSR not be == 0 if nothing has happened yet?
It's an interrupt status register.
My guess is that you mistook that one with the DMA software reset?
/* DMA Software Reset */
/* set SWR bit: resets all MAC subsystem internal registers and logic
* NOTE: the SWR is not performed if the ETH_RX_CLK or the ETH_TX_CLK are
* not available -> check external PHY or IO configuration
*/
ETH->DMAMR |= ETH_DMAMR_SWR;
/* wait for software reset to reset... */
u32TickStart = HAL_GetTick();
while( (ETH->DMAMR & ETH_DMAMR_SWR) == ETH_DMAMR_SWR )
{
/* timeout ? */
if( (HAL_GetTick()- u32TickStart ) > ETH_TIMEOUT_SWRESET_MS )
{
#if DEBUG_ETHNETIF_ERR
uart_printf(SZC_TEXT_ERR "ETH_DMAMR_SWR software reset timeout\n\r");
#endif /* DEBUG_ETHNETIF_ERR */
return HAL_TIMEOUT;
}
}
Another thing:
Interesting that you can talk to the PHY before enabling the MAC clock, I thought the MDIO works with that clock.
2026-03-04 8:53 AM
By the way have you seen this? https://www.linkedin.com/posts/tolylebedev_stm32-ethernet-explained-mac-phy-rmii-share-7434996521127022592-qdv5
2026-03-04 8:58 AM
If you have generated a project from scratch in CubeMX, it isn't guaranteed to work. Start from some ready example from the Projects subdir in the Cube package, or from here.
2026-03-04 11:59 AM
Hello LCE, Pavel A,
First, thank you all for the incredible support so far. I've made significant progress based on your advice and would appreciate your guidance on the next steps.
Following the excellent suggestion about the RMII reference clock, I:
Configured MCO1 (PA8) to output 50MHz from PLL1Q with divider /5 (240MHz → 48MHz)
Verified PA8 is set as MCO1 in the pinout configuration
Confirmed the clock tree now shows 48MHz output on MCO1
Despite the clock configuration, the Ethernet MAC still shows no signs of life:
Pre-RTOS: UART is working!
About to start RTOS...
LWIP task STARTING...
Manually configuring PHY...
Pre-RTOS: UART is working!
About to start RTOS...
LWIP task STARTING...
Manually configuring PHY...
Link established!
ETH power-up sequence...
All ETH clocks enabled
ETH reset released
ETH DMACSR after reset: 0x00000000
ETH still not responding - trying system reset
ETH DMACSR after system reset: 0x00000000
RxDesc: 0x30040000, TxDesc: 0x30040100, RxBuffLen: 1536
ETH HAL Init FAILED with error: 1
Setting up network interface...
IP set to: 192.168.1.110
Network interface is UP
Starting echo servers...The DMACSR register remains stubbornly at 0, indicating the MAC is not receiving any clock.
:white_heavy_check_mark: PHY is alive - Link LED is on, and we successfully read PHY registers via MDIO
:white_heavy_check_mark: MCO1 is configured - Clock tree shows 48MHz output
:cross_mark: MAC is dead - DMACSR = 0, MACVR = 0, DMA software reset times out
Please advise.
2026-03-04 12:00 PM
Thank you, will do
2026-03-04 12:00 PM
Great I am trying it now
2026-03-04 11:27 PM - edited 2026-03-04 11:32 PM
> DMA software reset times out
Wait, you say you want to configure MCO to 50 MHz, but are happy with 48 MHz ?
If this is about RMII REF CLK between PHY and STM32: you must have 50 MHz, not only something close to that.
This clock can also be supplied by the LAN8742.
Check the 750-DK schematics if the PHY pin "nINT/REFCLKO" has a pull-up, and check with a scope what's going on there.
And STM32 internally, you should supply the ETH MAC with at least 100 MHz (not 100% sure though).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.