2025-05-15 7:32 AM - last edited on 2025-05-16 1:07 AM by mƎALLEm
After adding in the .ioc file, in software package, Touch GFX and enabled grafic applications. when I try to lunch ApplicationTemplate.touchgfx.part i receive the following error message. Brlow i also put the content of the log file
Sorry - something unexpected has happened which caused an error to occur in the Designer.
For more information, see the log file located at: C:\Users\vdalessandro\AppData\Roaming\TouchGFX-4.25.0\TouchGFXDesigner.log
Please consider reporting this bug and steps to reproduce it at the TouchGFX Help Center so it can be fixed in a future version.
You can find the Help Center here: https://community.st.com/touchgfx
Error: Object reference not set to an instance of an object.
2025-05-15 10:35:12,492 [1] ERROR TouchGFXDesigner.App: Object reference not set to an instance of an object.
System.NullReferenceException: Object reference not set to an instance of an object.
at TouchGFXDesigner.Main.Project.Configuration.FeatureConfig.FeatureConfigCategory.UncheckFeaturesBasedOnSTMFamily(IEnumerable`1 allFeatures, String family, String subFamily)
at TouchGFXDesigner.Main.Project.Configuration.FeatureConfig.FeatureConfigCategory.InitializeFeatureGroups()
at TouchGFXDesigner.Main.MainWindowViewModel.InitializeFeatureGroupsWhenCreatingNewProject()
at TouchGFXDesigner.Main.MainWindowViewModel.LoadApplication(LoadApplicationEvent loadApplicationEvent)
at ApplicationEvents.ApplicationEvent.Raise[T](T args)
at TouchGFXDesigner.Main.MainWindowViewModel.ViewLoaded(FileInfo file)
at TouchGFXDesigner.Main.MainWindow.MainView_OnLoaded(Object sender, RoutedEventArgs e)
2025-05-15 11:39 PM
You need to open the file with extensions .touchgfx, not the .touchgfx.part
Also, please use the "code formatter" here to format your LOG in the post, to make the conversation more clear
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.