2020-07-29 5:45 AM
2020-07-29 6:23 AM
Hi @EnricoP
Welcome in this community.
For your information you posted initially your question under topic "STM32 MPUs" which address only STM32MP1 product family.
I retagged your post with STM32 MCUs, STM32H7, TouchGFX topics in order to reach relevant skilled people for you post.
Olivier
2020-07-30 6:28 AM
Hi,
Are you new to TouchGFX Designer? If yes, please have a look at the TouchGFX documentation. There is a tutorial available and more documentation on how to develop your project which can help you get started.
We have made an application template for the STM32H747I-DISCOS. So start you project by opening TouchGFX Designer and select the right AT, then generate code. In your project folder a configured CubeMX project will be created, with a CubeIDE project generated under the folder STM32CubeIDE.
Videos of a TouchGFX workshop have been recently uploaded on youtube, but it is not on your board and quite long. The 5th part is where the hand on examples start.
/Romain
2020-07-31 8:44 AM
thank you Roman!
I have made myfirstapplication with touchGFX, select AT STM32H747I-DISCO, and then generated code, but in TouchGFX folder I don't find any project folder with the code for STM32CubeIDE.
I want make an application that toggle a led (GPIO pin) on board STM32H747I-DISCO with a touch button on display.
Enrico
2020-08-03 1:59 PM
For some reason, there is no CubeIDE-project or CubeMX-project generated by TouchGFX when using the STM32H747I DISCO template. It is generated when selecting other board templates though.
When creating a cubeIDE project, the option to integrate TouchGFX is not available for this board
it's not available because the microprocessor has two cores ans it'snt support in touchgfx 4.13.0 ?
There is another method to do this?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.