STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Does the Scroll Wheel have a scroll bar?

I am sorry if this is a stupid question, but I have been looking for a way to enable the scroll bar on a Scroll Wheel widget. Does this widget have scroll bar functionality?My project will not use touch, so I am intending to use the Scroll Wheel inde...

scottSD by Lead
  • 2596 Views
  • 4 replies
  • 0 kudos

Converting char[] pulled from keyboard to an uint16_t

I know this seems like a simple question, but for whatever reason this is what is giving the most issues today.Here is what I am working with: Unicode::UnicodeChar keyboardBuffer[7][3];Unicode::UnicodeChar* buff = keyboard.getBuffer();  Unicode:: str...

DElli.1 by Associate III
  • 2397 Views
  • 2 replies
  • 0 kudos

why? TouchGFX compiler throws this error Core/Src/main.c:25:10: fatal error: fatfs.h: No such file or directory #include "fatfs.h"

I am developing a small project to which I decided to add a USB-HOST in MSC (Mass Storage Class) mode, with the intention of adding a USB pen drive, obviously I require the use of FATFS (USB-DISK mode) drivers. However, the Touch v4.14 compiler gave ...

Resolved! STM32F7 LCD flickering peoblem

Hi,I'm working on a project with STM32F746 and touchGFX. When I move (use move mixing) some widget witch its alpha value isn't 255 or change screen, the screen is flickering. I'm using an external frame buffer(SDRAM) and I did LTDC layer settings as ...

Flickering issue on STM32F769NI

Hi ,I am working with STM32F769NI based custom board with 7" display of 800 x 480 resolution. I am experiencing the flickering effect whenever I am trying to update the screen content with digital clock updated at every 1 sec.Please find the below vi...

Shree by Associate II
  • 1058 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.