2020-08-03 8:20 AM
Dear All,
It's the first time that I'm using ST Tools. I bought an evaluation board ( STM32F746G-DISCO ) because I want to test the Graphics tool TouchGFX. Following some tutorial I can load some graphics applications only made with this tool.
The problem now is that I would like to use both TouchGFX and STMCubeIDE for the same project but I can't find a way to do this. Online there are some tutorials made by hobbist but they don't work .
Is there an official document / guide / tutorial or example made by ST which explains the right procedure?
Thank you in advance,
Mattia
2020-08-03 12:21 PM
In the TouchGFX interface, after you run the Generate Code process, you can click on the Browse Code button in the bottom right of the screen to get to the generated code which takes you to the TouchGFX folder. If you go up one folder, you should find a STM32CudeIDE folder with a .cproject file there. Double click on this find and it should open in STM32CubeIDE where you can build and run the code on the board.
However, you might find this video helpful:
https://www.youtube.com/watch?v=o42r4xXOnbo
This one shows how to go from TouchGFX to STM32CubeIDE
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.