STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How do you implement a popup (container including some basic widgest) on EVERY SCREEN which can be set visible by the model?

Hi,I'm currently building a Touchgfx interface consisting of multiple screens (30+).Everything is working fine so far, however now I need to implement some sort of popup/warning dialog which can be triggered by the model.Each page needs to have this ...

H7 by Associate II
  • 2157 Views
  • 3 replies
  • 1 kudos

Black Screen after 4-5 Reboot

Hello,I'm using STM32H750IB (touchgfx 4.13.0 with freertos  V10.2.1) to control RGB TFT LCD, with external flash and also external SDRAM.The application runs well but sometimes (after 4-5 reboot) the screen remains black, if I reboot the application ...

Ngard.1 by Associate
  • 954 Views
  • 1 replies
  • 0 kudos

Resolved! Posible bug in Touchgfx Keyboard ?

Hey, I'm working on custom board Touchgfx project and I'm using Keyboard widget for text input. During testing I found out that keyboard Cancel event is not working properly.Description of problem: When i click and hold on one of keys and drag out of...

JLakn by Associate II
  • 4054 Views
  • 5 replies
  • 0 kudos

how to set up LTDC Hsync,Vsync and porch value???

hi.​I am using STM32F767 to control RGB TFT LCD. Data is output on the screen with TouchGFX.But sometimes the screen momentarily breaks for a very short period of time and then comes back.​When I changed the porch value of LTDC, the cycle of symptoms...

0693W000005ABMNQA4.png
ikassma by Senior
  • 3335 Views
  • 3 replies
  • 0 kudos

Resolved! X-NUCLEO-GFX01M1 and NUCLEO-F446RE: External Loader

I'm trying to port the STM32G071 NUCLEO DEMO downloaded via TouchGFX Designer 4.15.0 to the NUCLEO-F446RE.In order to use the external SPI Flash memory on the X-NUCLEO-GFX01M1 I need the external loder for the STM32F4 processor.The project downloaded...

ALomb by Senior
  • 2160 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.