2019-08-28 5:30 AM
Hi,
I'm currently building a Touchgfx interface consisting of multiple screens (30+).
Everything is working fine so far, however now I need to implement some sort of popup/warning dialog which can be triggered by the model.
Each page needs to have this dialog and I'll probably build it of a container and some basic widgets.
How would you implement this without adding the container on every single screen?
This seems like it's way to much work considering I'd also need to maintain the MVP structure for each view.
Thanks
Michael
Solved! Go to Solution.
2020-11-19 4:14 AM
Please look at a project i shared that shows you how to do base-views in a base-class, shared between screens. Currently there's no way of doing this in the designer, but it is coming. If you study that example i posted, you should be able to adapt it to your own project.
/Martin
2020-11-06 6:01 AM
I’ve got similar issues. Did you ever find a solution to this?
2020-11-19 4:14 AM
Please look at a project i shared that shows you how to do base-views in a base-class, shared between screens. Currently there's no way of doing this in the designer, but it is coming. If you study that example i posted, you should be able to adapt it to your own project.
/Martin
2020-11-19 4:57 AM
Hi Martin,
thanks for your response. Could you please link in one of your shared projects? I can't find them.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.