STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

How to configure a custom size with ILI9341 LCD ?

Dear TouchGFX Team,first of all, thank you for providing a great tool for top notch graphics. I'm happy to play with it, and learning about gfx basics from your resources was definitely most valuable input for me. Since I don't have any demo boards a...

PKriv.1 by Associate III
  • 6337 Views
  • 9 replies
  • 0 kudos

TouchGFX Double Framebuffer Swapping Logic

I'm a bit confused about the strategy used to determine when to swap buffers when TouchGFX is configured for double frame buffers. As illustrated here, the intent of the double frame buffer is to allow the old frame buffer to be presented if there is...

0693W000005AWzkQAG.png
Jon Enz by Associate III
  • 6936 Views
  • 8 replies
  • 0 kudos

Conflicting definition of HAL_DCMI_Init?

I'm experiencing a runtime crash when using DCMI in with `USE_HAL_DCMI_REGISTER_CALLBACKS`.The crashing lines are#if (USE_HAL_DCMI_REGISTER_CALLBACKS == 1) /*Call registered DCMI line event callback*/ hdcmi->LineEventCallback(hdcmi); #else ...

Dan Rose by Associate II
  • 1596 Views
  • 3 replies
  • 1 kudos

[TouchGFX] New TFT on 32F429IDISCOVERY board

Hello,I managed to connect several displays on a custom PCB (similar to 32F429IDISCOVERY) using several drivers (ILI9344,ILI9488 etc) and running the TouchGFX library.Now, I have a problem with a new one. It supports RGB directly but has no DE (data ...

SKokk.1 by Associate II
  • 2168 Views
  • 2 replies
  • 0 kudos

I receive no errors while compiling the header file( attached in details), for a LCD interface, but as I include this header in my .c file a lot of errors and warnings appear. I am new in c and HAL, kindly give some detail or reference for knowledge base

* S6D0154_LCD.h * * Created on: 16-Nov-2020 *   Author: NUCLEO */#ifndef INC_S6D0154_LCD_H_#define INC_S6D0154_LCD_H_#include "stm32f103xb.h"#include "stm32f1xx_hal_gpio.h"typedef struct{ uint16_t pin; // LCD Pins interface to STM32. GPIO_TypeDef ...

WRaso.1 by Associate II
  • 4378 Views
  • 5 replies
  • 0 kudos

STemWin is not working with IAR

Hello! I've noticed that STemWin from st.com does not work with IARv8.x. The reason is that in IAR wchar_t size is 32 bits and STemWin library has wchar_t size 16 bits. Is there any solution to this problem? Or STemWin is just incompatible with the n...

Resolved! Difference between TouchGFX Core Libraries

Hi @Martin KJELDSEN​ Hi @Alexandre RENOUX​ I have a general question. What is the difference between the touchgfx_core.a and the touchgfx_core_release.a library (both for Cortex M7)?. With the release version of the library our application crashes a...

Marco.R by Senior
  • 1483 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.