2020-11-19 12:49 AM
Hello,
I'm using STM32H750IB (touchgfx 4.13.0 with freertos V10.2.1) to control RGB TFT LCD, with external flash and also external SDRAM.
The application runs well but sometimes (after 4-5 reboot) the screen remains black, if I reboot the application starts correctly.
After some tests I found that the LTDC module goes in FIFO UNDERRUN when the black screen happens. SDRAM is initialize in the bootloader and the LTDC is initialize in the application.
How can I solve this problem?
Best Regards
Nicola
2020-11-19 3:56 AM
I'm not sure why it would happen after 4-5 reboots. Try reducing the pixel clock a bit to see if you're still having that issue. Or using hal.lockDMAToFrontPorch(true); in your TouchGFXHAL.cpp (initialize()).
This will overall reduce the strain on your memory bus.
/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.