2020-11-17 3:50 AM
I'm trying to port the STM32G071 NUCLEO DEMO downloaded via TouchGFX Designer 4.15.0 to the NUCLEO-F446RE.
In order to use the external SPI Flash memory on the X-NUCLEO-GFX01M1 I need the external loder for the STM32F4 processor.
The project downloaded via TouchGFX Designer 4.15.0 provides the external loader MX25L6433F_STM32G071B_NUCLEO.stldr in binary format.
Is it possible to have the external loader project so that it can be adapted to other STM32s (STM32F446 in my case) ?
Or I have to necessarily implement it from scratch, maybe I get started on the MOOC "How to create an external QSPI loader MOOC" ?
Solved! Go to Solution.
2020-11-18 8:32 AM
I have implemented the external loader !
If it helps, in addition to the MOOC link, I referenced the following links:
and the demo project in C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\ExternalLoader directory.
Many thanks to @Tilen MAJERLE !
Attached the stldr
2020-11-18 8:32 AM
I have implemented the external loader !
If it helps, in addition to the MOOC link, I referenced the following links:
and the demo project in C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\ExternalLoader directory.
Many thanks to @Tilen MAJERLE !
Attached the stldr
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.