STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

I'm trying to get a TFT display to work using Touch GFX on a custom board. Why doesn't the display I make in touch GFX show up?

320x240 Parallel RGB (LTDC) interface. I've been following the TouchGFX board bring up instructions. I can change the background color, so the hardware side should be good.I made a display in TouchGFX, everything compiles. TouchGFX updated the files ...

0693W00000Y9ypSQAR.png 0693W00000Y9yqGQAR.png 0693W00000Y9yquQAB.png 0693W00000Y9yrdQAB.png
SWood.4 by Associate III
  • 4515 Views
  • 9 replies
  • 0 kudos

Resolved! LTDC: Display Compatibility Question

Hello,I am looking to use the LTDC (LCD-TFT) feature to interface with a TFT display and potential touch controllers (CTP). I am uncertain on the requirements to interface with it and wanted to confirm a few details.I have written software (generated...

KMew by Senior III
  • 3252 Views
  • 4 replies
  • 0 kudos

Resolved! Black horizontal lines when SDRAM is used. Why?

Hello,another day, another problem...I just started with a custom board. But i am using parts which are already working on boards from ST so i thought it will be easy to adapt.I started a new project and if i use internal RAM for a touchgfx box every...

0693W00000Y9GIFQA3.jpg 0693W00000Y9GI5QAN.jpg 0693W00000Y9GI0QAN.jpg

DMA2D transfer error causes touchgfx to fail to work properly. How to solve the problem of UI screen stuck?

During the normal operation of the program, after touching the pin on the external sdram by hand, the UI screen is stuck. The simulation shows that the DMA2D Transfer error flag is set, touchgfx cannot work normally, and the chip works normally after...

L丶zs by Associate II
  • 1855 Views
  • 2 replies
  • 0 kudos

Resolved! "Run-Simulator", Compiler, Where can I suppress the error "...may be undefined [-Werror=sequence-point]"?

TouchGFX 4.21.1When compiling for "Run Simulator" I get the following error message:Run Simulator  Generate    Wrote generated/simulator/gcc/Makefile    Done  Generate Assets    make -f simulator/gcc/Makefile assets -j10 -Wno-error=sequence-point    ...

Roger.ch by Associate III
  • 3294 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.