2023-02-09 10:18 AM
I want to add another dislay(replace another) display with my STM32F7508-DK board which uses different LCD Driver ID as opposed with the offthe shelf Dev kit, What is the process of that, How can we achieve the required functionality if Considering Pins are compatable just the Size of LCD is 7" as opposed to 4.2" and controller id is also different
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.