2023-02-08 10:01 PM
Hello,
In my project I need to connect BW 10b camera to STM32U585.
STM32U585 is running at 160MHz, and my MCO for camera is 10-30MHz. At this point I am not even using DMA, just checking DCMI interrupts
And what do you know, first, I get OVR interrupt, and when I get HSCYNC, VSYN IRQ and they do match what camera is trying to output.
void DCMI_Config(void)
{
DCMI->IER =DCMI_IER_OVR_IE|DCMI_IER_VSYNC_IE;
DCMI->CR =DCMI_CR_ENABLE | DCMI_CR_HSPOL |DCMI_CR_PCKPOL| DCMI_CR_VSPOL | DCMI_CR_DR_SIZE_10b;
NVIC_SetPriority(DCMI_PSSI_IRQn, 1);
NVIC_EnableIRQ(DCMI_PSSI_IRQn);
DCMI->CR |=DCMI_CR_CAPTURE;
}void DCMI_Interface_Init(void)
{
LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOA);
LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOB);
LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOC);
LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOD);
LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOE);
LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_DCMI_PSSI);
/*
PB6 ------> DCMI_D5
PE4 ------> DCMI_D4
PC12 ------> DCMI_D9
PC10 ------> DCMI_D8
PE6 ------> DCMI_D7
PB8 ------> DCMI_D6
PB7 ------> DCMI_VSYNC
PA9 ------> DCMI_D0
PA10 ------> DCMI_D1
PC9 ------> DCMI_D3
PC8 ------> DCMI_D2
PD9 ------> DCMI_PIXCLK
PA4 ------> DCMI_HSYNC
*/
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
GPIO_InitStruct.Pin = LL_GPIO_PIN_9|LL_GPIO_PIN_10;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_4;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Alternate = LL_GPIO_AF_10;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_6|LL_GPIO_PIN_7;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Alternate = LL_GPIO_AF_10;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_12|LL_GPIO_PIN_10;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Alternate = LL_GPIO_AF_10;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_9;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Alternate = LL_GPIO_AF_4;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_9;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Alternate = LL_GPIO_AF_10;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOD, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_5|LL_GPIO_PIN_4|LL_GPIO_PIN_6|LL_GPIO_PIN_0;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Alternate = LL_GPIO_AF_10;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOE, &GPIO_InitStruct);
}Based on datasheet, DCMI can run at 64MHz (Frequency ratio DCMI_PIXCLK/fHCLK=0.4), while I only do 10-30MHz, and yes, I checked with scope.
Same goes to M33 core frequency, it is 160MHz.
Errata is also not say anything. Porting this code from STM32L4, and it was working like a charm.
2023-02-08 11:50 PM
> At this point I am not even using DMA
That's why you get overruns. Data are churning in into DCMI's FIFO, you have to pull them out from the mcu side at the same rate.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.