STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Couldn't reserve space for cygwin's heap

Hi,using TouchGFX, I get the following error when I run the code.How can I fix this?Thanks***************************************************************Compiling simulator/main.cppCompiling touchgfx/framework/source/platform/driver/touch/SDL2TouchCo...

AndreaTW by Associate II
  • 564 Views
  • 1 replies
  • 0 kudos

Resolved! Font not discovered in ./assets/fonts

Hi,Using Designer 4.25, I copied a font to ./assets/fonts folder but it is not in the list"Solido Compressed W00 Bold.ttf"Name displayed by OS is "Solido Compressed W00 Bold" when open in FontForge Any idea how to make the Designer to recognise the f...

ferro_0-1743415790407.png ferro_1-1743415823191.png
ferro by Lead
  • 1058 Views
  • 3 replies
  • 3 kudos

Resolved! TouchGFX for custom display

HI,I´ve to design a solution with a custom 5 and 7 inch color displays for a more or less static graphics (just some values and maybe some charts).Which interface / MCU would you recommend? MIPI-DSI? Would be fine to have a quite small MCU (preferrab...

AWack by Senior
  • 765 Views
  • 4 replies
  • 0 kudos

Riverdi 121STM32H7 linking problem with Keil

Hello I have a problem compiling TouchGFX for Keil. My procedure:1/ Run TouchGFX Designer 4.252/ Create New project3/ Go to tab – By Partners – select board Riverdi STM32 121STM32H74/ Click to Create5/ Add Button ( for example)6/ Click Generate CODE7...

riverdi.jpg riverdi3.jpg riverdi4.jpg
mcumake by Associate II
  • 4463 Views
  • 26 replies
  • 1 kudos

Resolved! JPEG Gui icon without Touch GFX on stm32h7

hi,I am currently using BMP + rgb565 LTDC display for GUI icon creation without Touch GFX ( Everything is on "" C"" only and Manual preparation icon using hex converter ).Already known one is ! for a small size ,BMP is OK but large size BMP icon  wil...

MMARI1_0-1755258457457.bmp MMARI1_1-1755258542949.bmp
MMARI.1 by Senior II
  • 1353 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.