2025-11-13 10:15 PM
HI,
I´ve to design a solution with a custom 5 and 7 inch color displays for a more or less static graphics (just some values and maybe some charts).
Which interface / MCU would you recommend? MIPI-DSI? Would be fine to have a quite small MCU (preferrable no BGA or WLCSP)
Best regards,
Achim
Solved! Go to Solution.
2025-11-19 1:47 AM
Hi @AWack ,
It depends on your resolution, and the quality of the visuals you want to show. Let's say you have a 320*480px resolution using 16 bit color depth and 1 full framebuffer , you will need 320x480x16/8 x1 = 307,200 bytes available in internal RAM.
LCD-TFT is just a preference of mine. With TouchGFX, LTDC are supported very easily and it's well documented. But DSI displays can also be used of course.
2025-11-18 1:38 AM
Hello @AWack ,
You can see our portfolio here and select the right MCU depending of your technical needs. I would personally recommend to select an MCU with sufficient internal RAM to store at least 1 full framebuffer (if you don't expect any animation, 1 framebuffer is enough, you don't really need 2). Also If you want simpler integration, I would recommend using LCD-TFT instead of MIPI-DSI.
2025-11-18 10:52 PM
Hi Osman,
thanks for your reply! Could you give me an example for the size of the frame buffer?
What´s the reason you would prefer LCD-TFT instead of MIPI-DSI? Is the frame buffer size also applicable for DSI?
Best regards,
Achim
2025-11-19 1:47 AM
Hi @AWack ,
It depends on your resolution, and the quality of the visuals you want to show. Let's say you have a 320*480px resolution using 16 bit color depth and 1 full framebuffer , you will need 320x480x16/8 x1 = 307,200 bytes available in internal RAM.
LCD-TFT is just a preference of mine. With TouchGFX, LTDC are supported very easily and it's well documented. But DSI displays can also be used of course.
2025-12-04 5:54 AM
Hello @AWack ,
Do you need more info or is this clear for you?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.