STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Detect any touch

Hello,I developed a product,but customer wants that if no touch detected in 10 seconds the device will go in home page. I believe that the only way is to manage STM32TouchController.cpp in the point I have higlighted  Is it the best way ?Thankyou for...

MauFanGilaMedical_0-1764747915219.png

Custom STM32 project with TouchGFX

Hi all, My goal is to develop a personal STM32 + TouchGFX project.I’m reaching out to you because I’ve gone through all the tutorials, YouTube videos, GitHub repositories, ChatGPT, etc., without finding a solution.I followed the tutorial ''https://w...

PSpee.2 by Associate II
  • 1075 Views
  • 3 replies
  • 0 kudos

touchgfx and usb msc

hello, I need to use both touchgfx and usb msc host with stm32h743 in my project. they work fine separately , but when I add usb to my touchgfx project it does not work(all my usb implementations are based on controllerstech video). Do I need to do a...

Zakba.1 by Senior
  • 2094 Views
  • 5 replies
  • 0 kudos

Resolved! Multi-level menu

Hi all,I would like some ideas/help with designing an interface for a large multi-level menu. I need the user to be able to get to specific information about a vehicle make, model and year. My first thought was to use a scroll list or wheel for the u...

SGill.3 by Associate II
  • 3787 Views
  • 4 replies
  • 3 kudos

Resolved! boxProgress orientation, and circleProgress size

Hi, In my UI project I need a vertucal boxProgress while all available backgrouds and images are horizontal while w&h are greyed out. When I create a custom background, the progress bar is not working. Same for circleProgress (size control). Can you ...

ksale.1 by Senior II
  • 592 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.