cancel
Showing results for 
Search instead for 
Did you mean: 

Color Eyedropper tool for flexButton cannot be toggled off when selecting another window

noahl
Associate

Hello!

I'm working with the flexButton tool and wanted to change the color via eye-dropper. But once I turned on that option, I was unable to turn it off, I can't disable the color picker and it continously changes the color even after deselecting. 

 

Isolating the cause a bit I realized it only happens when I move my cursor off screen into another window and click, operating the tool normally (staying within touchGFX window) correctly turns off the tool after selecting. 

Just a bug I noticed,

Thank you

1 REPLY 1
JohanAstrup
ST Employee

Hello @noahl.

However, I have not been able to reproduce it. I followed this procedure:

  1. Create a new simulator project in TouchGFX Designer.
  2. Insert a Flex button.
  3. Navigate to Box With Border and select the Eyedropper for the released background color.
  4. Click in another window (I have also tried clicking another window on a different screen).
  5. When I click, the properties pop-up immediately closes, and the color is no longer changed.

Could you share the procedure you followed if it deviates from the one described above?

I used TouchGFX 4.26.0. Which version of TouchGFX did you experience the issue in?


Best regards,
Johan

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.