STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Handling an input signal within 1 ms

Hello,I have to measure the pulse width and the period of Fiber-Optical Signal with STM32F469 Discovery board and view the values on the display using TouchGFX Design.I have no problem to blocking the display for a while (max. 2s) to read a pulse wid...

signal.png
mids400 by Associate III
  • 3750 Views
  • 8 replies
  • 3 kudos

Resolved! LTDC not generating clock

Hi,I have a Nucleo-U5A5ZJ-Q board which i replace the mcu with a STM32U5A9ZJT6.I'm trying to use LTDC to control a 800x480 LCD (WF50FTYAGDNN0#) via RGB888.Eventually running touchgfx, but I have fallen over at the first hurdle.I have read many tutori...

PhilipC by Associate III
  • 11062 Views
  • 14 replies
  • 9 kudos

Read data from sd card in touchgfx

hi im using f746g-discovery board i want read image data from sd card and display it on screen. but i dont know how can read data from sd card and how display it on screen. Thank you for reading.

ahnm002 by Associate
  • 1395 Views
  • 1 replies
  • 0 kudos

TextArea and Keyboard.

1) How can I make the TextArea widget clickable and handle the PRESSED and RELEASED events separately?2) How to create a keyboard? When the TextArea is clicked, the keyboard appears, numeric data is entered, and it closes. Is there an example of a pr...

slavaglow by Associate II
  • 1745 Views
  • 1 replies
  • 1 kudos

Resolved! touchgfx print Unicode para o caractere "♂" 0x2642

Hello everyone,I spend hours trying to print the male and female ♂ ♀ symbol on the screen, without success.I tested this code and it works perfectly, when I change the hex to the desired symbol does it print "?" Screen1ViewBase::setupScreen(); ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.