STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! setAlpah issues

hi guys im having an issues with opacity of a picture in the touchGFX from some reason its giving me only tree option: solid (255) or invisiable (0),and the third option is between which is staying on the same opacity all around the scale between 1- ...

shalevBA by Associate
  • 1482 Views
  • 1 replies
  • 0 kudos

Resolved! Swipe Container

hi,1- What's the best way to speed up the swipe container transition?2- How can I change the animation of swipe container? 3- SwipeContainer.cpp can not modify. how do I make changes permanently ?  thanks for help 

snnzdmr1 by Associate III
  • 1627 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to flash the STM32U5G9J-DK2

Hi. Updates:1) Cancelled our original order with DK due to the ECCN delays. Did receive a notice from the open ticket with ST support that the ECCN issue has been resolved with DK. Mouser did not have this delay so ordered the tool from their store.2...

Mon2 by Senior III
  • 3141 Views
  • 3 replies
  • 0 kudos

Resolved! TouchGFX text translations typed text ID

Im trying to use the TouchGFX designer "text & translations" as a database of sorts.I've tried to use the function getText(text id) from the Reference but i'm not able to locate the text ID. The code below is from the TouchGFX framework.const touchgf...

AlX1TDf
XD by Associate III
  • 3571 Views
  • 3 replies
  • 1 kudos

Resolved! How to enable External Data Reader and DMA2D (TouchGFX)

Hello everyone,I encountered a problem while using TouchGFX. I want to use an external Flash which is connected via QUADSPI.The Flash works fine (manually loading and writing some informations into the memory). Block mode, Memory Mapped mode, both do...

MWetter by Associate III
  • 4377 Views
  • 5 replies
  • 0 kudos

Resolved! F746 custom board

Hello,I made a custom f746 board like it is done on the discovery board. I have only implemented SDRAM and QuadSPIFlash. I can program the mcu without any problems. The display flickers heavily  https://youtube.com/shorts/pYuCkyMqsgM?si=iGS41lJvxs_Cg...

MReus.2 by Associate II
  • 2171 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.