STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX 4.23.1 release notes

Hello everybody,where can I find the release notes of the TouchGFX Designer tool ? In particular I'd like to know the Release notes of ver 4.23.1 and the differences between 4.23.1 and 4.23.0.Thanks Max

MaxC by Associate III
  • 1436 Views
  • 1 replies
  • 0 kudos

ToggleButtons - hw buttons

Hello,i have an app that will only be controlled by hw buttons.I have several ToggleButtons on the configuration screen. When I use the -> and <- arrows (hw buttons), I step over the buttons on the screen one by one. I can find out which button I am ...

JNova.0 by Associate III
  • 986 Views
  • 1 replies
  • 0 kudos

Resolved! custom widget

if I make my own widget, can it be added to the palette among the supplied widgets?The second question is about the properties panel. I can somehow configure it for a custom widget and put my widget parameters on it.If it cannot be added to the widge...

JNova.0 by Associate III
  • 1755 Views
  • 1 replies
  • 0 kudos

Migration from emWin to TouchGFX

I'm currently switching from the emWin 5 graphics library to TouchGFX and have a question.I have an IMAGE widget that reacts to an event: 1) click (calls a function to play sound) and 2) release (calls a function to send data to change status: SET_ST...

slavaglow by Associate II
  • 1779 Views
  • 1 replies
  • 0 kudos

Resolved! draggable circle

Hello,I would like to enable the dragged of the circle only in the horizontal direction for a customized container on which I only have a circle. I would also need to limit the left and right "stop" when dragging. I set up draggable and I can move th...

JNova.0 by Associate III
  • 1924 Views
  • 1 replies
  • 1 kudos

Black screen initial display start problem

I have an H755 nucleo board and a riverdi 5'' rgb display.Aftersetting the ltdc ,the clock to 25mhzthe freertosnot using qspi and sdram just by using the 2 layer start address 0x20000000 and 0x20119400 for RGB888I have enabling the nvicI have crossch...

Kyrpav_0-1706266487249.png Kyrpav_0-1706305583400.png Kyrpav_1-1706305593696.png
Kyrpav by Associate III
  • 1894 Views
  • 0 replies
  • 0 kudos

Resolved! Customized circle progress

Hi,I'm looking at customising the circle progress.I was able to add this as the background image and added a single dot as the image to rotate.Any idea on how to rotate the dots and make it disappear? 

KNara2_0-1704292274992.png KNara2_1-1704292433716.png
KNara.2 by Associate III
  • 5144 Views
  • 7 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.