STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How to save a circle color when change to another screen

Hello all, I have made a GUI with some circles that show as a LED. When the LED must be turned on the color of the circle shall be green and LED is OFF then the color must be changed to gray. So when I change the screen to another and back again, the...

ayoub_0-1714722025210.png
ayoub by Associate II
  • 3610 Views
  • 6 replies
  • 1 kudos

Resolved! Getting data from List Layout Elements

I am not very experienced with CPP or TouchGFX. I have created a Custom Container with a TextArea, a ToggleButton, and a couple of ScrollWheels. I have created a list layout, and used .add() to add two new instances of the Custom Container to my list...

CYBR by Associate II
  • 2601 Views
  • 2 replies
  • 0 kudos

See if the Init Code conversion is correct?

It received the initial code for the ILI9806E.The codes you received are as follows.write_command(0xFF); // Change to Page 1 CMD write_data(0xFF); write_data(0x98); write_data(0x06); write_data(0x04); write_data(0x01); write_command(0x08); //Output S...

PKunK.1 by Associate III
  • 3741 Views
  • 5 replies
  • 0 kudos

Resolved! Resize string variable

Hi i have this code: char string[6]="Hello";char string1[6]="World"; touchgfx::Unicode::UnicodeChar dst[6];touchgfx::Unicode::UnicodeChar dst1[6];touchgfx::Unicode::UnicodeChar txtAreaBuffer1[100]; Unicode::strncpy(dst, string, 6);Unicode::strncpy(ds...

Schamann by Associate II
  • 2018 Views
  • 3 replies
  • 0 kudos

Resolved! Portrait readBMP24File

My problems with Portrait orientation don't end.I have a very large project where changing the architecture and function calls costs much more than changing a single function.My problem is how?The function is readBMP24File.In my project it is loaded ...

Resolved! TouchGFX change button text

Hello, I try to do my own keyboard.My idea: when click on shift button (red a, btnShift) i want replace big letters with small. All buttons are FlexButtonCan I use the Action Execute C++ code ?like this:btnA.setText(TypedText('a'));but not woking now...

Schamann_0-1714601554516.png
Schamann by Associate II
  • 4143 Views
  • 4 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.