STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SBSFU | Option bytes programming and OpenOCD

Hello all,Another question from SBSFU series.I'm wondering what are the available ways to clear option bytes?The option I was using so far was simply STM32CubeProgrammer GUI, but what if we don't have ST-Link on board and we have to rely on something...

JakubStandarski_0-1695831702179.png

Resolved! Calling secure function from non secure area in TF-M threadx

Hi, need support. send_msg() is a secure area message of TF-M and I am calling it in non secure area via secure_nsc API.What I am observing here is that I am not able to call this function in _tx_initialize_kernel_enter() function after the call to T...

Nitin by Associate III
  • 2063 Views
  • 1 replies
  • 0 kudos

STM32 H733 Secure Boot & Secure Firmware Update

Hi,I need to implement things that are required to implement secure boot & secure software update STM32 H733 Microcontrollers. Trying to understand from the beginner perspective, though I have the Cube package downloaded from the st website, still li...

Issue with SFBU and EEPROM Firmware Update

Hello,I'm currently working on a project that involves using the SFBU (Secure Firmware Bootloader Update) due to the limited flash size of the MCU. I've set up an external EEPROM to store the entire firmware before the update process.I've made necess...

NAndreadakis_0-1700570215656.png NAndreadakis_1-1700570474151.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.