STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Using derived hardware key (DHUK) with AES on stm32u5

I've been trying to set up the AES peripheral so that it's only using the hardware derived key from the SAES peripheral (without setting any clear text key). However, the only method mentioned in the reference manual on using the DHUK is through the ...

jptuser44_0-1701456000989.png

Resolved! What could cause the crypto processor to freeze on STM32H750VB?

We are using STM32H750VBT6 rev V and have encounter boards with mcus that freezes when we try to use the CRYP.  So far we have seen that on failing boards the crypto registers are zeroed immediately after initialization but on a functional board ther...

URodi.1 by Associate
  • 3887 Views
  • 7 replies
  • 3 kudos

Resolved! STM32U5 SAES/AES shared key in Trustzone with HAL

Hello,I'm trying to use the SAES/AES shared key functionality in a Trustzone (TZEN=1, RDP = 0), using the functions provided by the HAL library. The board I use is the B-U585I-IOT02A.The only project example I found is with Trustzone disabled, but it...

ptrchv by Associate II
  • 3228 Views
  • 2 replies
  • 0 kudos

AES ECB initialization fails

Hi,I'm trying to encrypt and decrypt in my device, running on a STM32H753, using AES ECB.I'm initializing crypto like this:  hcryp.Instance = CRYP; hcryp.Init.DataType = CRYP_DATATYPE_8B; hcryp.Init.KeySize = CRYP_KEYSIZE_256B; hcryp.Init...

TVare.1 by Associate III
  • 4368 Views
  • 5 replies
  • 5 kudos

Resolved! secure firmware update using USART

Hi everyone,I'm working in a Medical devices company and we use currently plenty of STM32s (F0,F1,F4, maybe soon H7). Until now, we didn't bother that much the cybersecurity topic for the firmwares but now the norms are forcing us :D.I checked a bit ...

TKopp.67 by Associate II
  • 3582 Views
  • 2 replies
  • 0 kudos

Resolved! How to enable the STM32H750VBT6 HW crypto?

I've tried to enable the CRYPT and HASH peripherals by setting bits 5 and 4 in the AHB2ENR register, but all peripheral registers read as zero and writes are ignored as if the clock wasn't enabled or the peripheral was missing. Does this chip have ha...

JBram.1 by Associate II
  • 12181 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.