STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H523RCT6 READ OUT PROTECTION LEVEL1

Hi ST Team,                   Currently i am using STM32H523RCT6 mcu for one of my project. In this i want to set the read out protection of level 1. Currently i am using below sequence to set the read out protection of level 1 protection..    // Unl...

Resolved! STM32U5 TrustZone enabled DMA problem

I am using STM32U585 and I stumbled upon the following problem:If a device is configured with TrustZone enabled (TZEN=1) there is different behavior in the following situations:1. SPI is configured without DMA and CPU is running non-secure code in pr...

milorad by Associate III
  • 2993 Views
  • 3 replies
  • 1 kudos

Identifying System Reset Causes in SBSFU on STM32U575

Hello,I am using SBSFU on the STM32U5 microcontroller, and I have implemented a function to determine the cause of the system reset by reading the RCC register flags. However, every time I enter the function, it always returns an 'unknown reset' valu...

AoP by Associate
  • 1733 Views
  • 1 replies
  • 0 kudos

Resolved! Secure Update via USB Stick (STM32H750) SBSFU / QSPI

Hello to all,I was wondering if there was a way to implement a secure update via USB stick using X-CUBE-SBSFU software.Moreover, the application software would be installed on external flash, custom bootloader immutable in internal flash.Maybe instal...

i2399 by Associate III
  • 3818 Views
  • 6 replies
  • 3 kudos

Resolved! SBSFU installation issue

 Hi,I'm using F4 series board (STM32F423ZHT6). also I'm using F4 and scripts say L series - are they compatable?STM32CubeProgrammer version: STM32CubeProgrammer 2.14.0 - This is support SBSFUX-CUBE-SBSFU version: 2.6.2I follow the https://www.youtube...

Meenakshi_3-1727515888859.png
Meenakshi by Associate III
  • 1305 Views
  • 1 replies
  • 0 kudos

Resolved! How to implement secure boot on STM32 MCU

Hi,I'm using STM32F423ZHT6 MCU board. I want to implement the FOTA as well as Scure Boot on my EVAL board. But I don't have much knowledge about Secure Boot. So, I refer https://www.st.com/en/embedded-software/x-cube-sbsfu.html and AN5056. The SBSFU ...

Meenakshi by Associate III
  • 5605 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.