STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STSAFE-A110 and hardware-level security

I'd like to open a small discussion about what would be the best usage of STSAFE-A110 to enhance the hardware-level security of our IoT device. To be more specific, in our application we want to use the STSAFE-A110 to store the customized device priv...

naNEQ by Associate II
  • 1979 Views
  • 1 replies
  • 0 kudos

Enable TrustZone without using STM32Programmer

Hello,I am working STM32u575 Nucleo board. I want to use secure flash to store secure data and to use it I need to enable TrusZone. Is there a way we can program option bytes with TZEN =1 without using STM32programmer?Regards,Shafi

Shaffi by Associate II
  • 1632 Views
  • 2 replies
  • 0 kudos

Resolved! STM32U585:FLASH Read protection level 1 issue

Dear Sir/Madam We are using STM32U585AII6Q MCU part in one of our projects. We encountered a problem with Flash read protection and no longer able to flash the MCU. Below is the reference screenshot from the error. We also tried few methods defined ...

apoorvabs_0-1728648184182.png
apoorvabs by Associate II
  • 3023 Views
  • 4 replies
  • 2 kudos

Resolved! Need help on writing into secure flash in STM32U575

I am working on STM32U575 to write and read from Secure flash. I referred   STM32Cube_FW_U5_V1.4.0\Projects\NUCLEO-U575ZI-Q\Examples\FLASH\FLASH_EraseProgram_TrustZone\but I was facing following issueCan you please help me resolving it. Do we have an...

Shaffi_0-1728377891530.png
Shaffi by Associate II
  • 3746 Views
  • 7 replies
  • 0 kudos

RCC_CSR registers with SBSFU

Hello,I am working with SBSFU on a STM32U575 microcontroller and have written a function to check the cause of the system reset by reading the flags from the RCC registers using __HAL_RCC_GET_FLAG. However, the issue is that none of the RCC register ...

Resolved! SFI without TrustZone on STM32U5 is possible?

I need to perform SFI on an STM32U599 MCU, so following the wiki article "SFI Step-by-step on STM32 boards" I prepared the firmware and programmed the HSM V2 smartcard.I'm sending the commandSTM32_Programmer_CLI -vb 1 -c port=SWD mode=HOTPLUG -sfi xx...

paolog by Senior
  • 4117 Views
  • 7 replies
  • 0 kudos

SBSFU with wolfssl in stm32h7

Hi,I am trying to replace mbedTLS library with Wolfcrypt library for crypto operations in SECoreBin project of SBSFU. I was able to replace SHA256 related APIs. But the bootloader is crashing when I try to initialize wolfssl ECC key object under SE_C...

h_adi by Associate
  • 1094 Views
  • 1 replies
  • 0 kudos

Resolved! STLINK JTAG Vulnerability when RDP2

Hi @Jocelyn RICARD GreetingsWe have a query from our support team"known vulnerability in the STM32U5 series related to the JTAG lock when using RDP (Readout Protection) Level 2." Is it advisable to proceed with this implementation, or should we consi...

PJose.4 by Senior
  • 2382 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H750 External Flash Read Protect

Working on setting RDP (read out protection) on STM32H750.  We are using an external loader to be able to read from/write to external flash. The internal flash only contains a bootloader.1. Setting RDP to Level 1 doesn't prevent reading external flas...

SMoon.2 by Associate III
  • 2098 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.