STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! X-CUBE cryptolib in sbsfu

Hi,I am implementing the sbsfu encryption functionality on the stm32u575 micros which do not contain hardware accelerator. For this I have decided to use x-cube cryptolib to be able to encrypt and decrypt messages. I have tested the example aes_cbc_e...

Encountering an error while doing DA

Hi, I have accidentally set the option byte PRODUCT_STATE=0x17 and the device is locked and shows the following when I do DA discover.This is the log related to the error message.12:09:28 : Start Debug Authentication Sequence12:09:28 : SDMOpen       ...

Resolved! Derive key for ECDH

Hi everyone, I develop a asimmetric public/private key crypto scheme and then with simmetric derived ley establish a comms with HOST REMOTE  <-> [LOCAL HOST/STSAFE]. I generate with ephimeral slot with:ret_code = (int32_t)StSafeA_GenerateKeyPair(hand...

FMaro.1 by Associate II
  • 2586 Views
  • 2 replies
  • 0 kudos

Resolved! debug OEMiRoT-Boot project on U083 possible?

I'm aiming to use the OEMiRoT sample project as a concept for secure updating of a large single-slot application in STM32U083 (need application size at least 160kB for migration from STM32L071). For that I need to give the bootloader a driver for ext...

Hans_W by Associate III
  • 2481 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.