STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H563: Unable to Regress or Debug Authenticate

Hello,(previous post was marked as spam - I don't know why, so I'm posting again...)I've been working on Provisioning my STM32H563 and after 3 weeks of not touching it, I am unable to perform Full Regression or Debug Authentication on my password-pro...

Resolved! X-CUBE-SBSFU CAN bus support

Hi everybody!We have to implement firmware update feature via CAN interface. Our challenge involves implementing a secure and safe firmware update feature via the CAN bus, driven by regulatory requirements in the medical field. Unfortunately, the exa...

Vadym by Associate II
  • 5117 Views
  • 9 replies
  • 2 kudos

Resolved! SBSFU: encountering unexpected TLV error

Hi,I am evaluating/learning the SBSFU application example on STM32WBA55CG and having issues getting it up and running. Below is the screenshot of the example log:To begin with, I want to be able to do the following.1. Flash the bootloader and flash t...

mr_divakar_0-1738874549615.png

Resolved! STM32U0 OEMiRoT RDP regression appnote?

I'm trying to find out the exact steps to regress an STM32U083 to an erased state after programming it with the OEMiRoT example project and and locking it to RDP2 by the accompanying provisioning.bat script.Will be using STM32CubeProgrammerCLI (or th...

Hans_W by Associate III
  • 2084 Views
  • 4 replies
  • 0 kudos

STM Cryptographic Library V4 (CCM)

Good day.I use in my project transfer of information between devices, for encryption and authentication I use the CCM mode (self-written library) as the encryption base I use AES-ECB.A device from the G0 series was added to my project, STM Cryptograp...

CCM.png
peit by Associate II
  • 1335 Views
  • 0 replies
  • 0 kudos

Resolved! Debug autentification with certificate on STM32H563

Hi. How can i connect a debug session to a device with product-state: closed and non secure software (no TZ active) without full regression.   I have create the password.bin file and two certificate files with TrustZone Package Creator: - DA with p...

stm32cubeide_rV2jj6lTVp.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.