STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! TrustZone TFM Example Problems

We have a project where we're using a U5A5 MCU with trustzone enabled and we're currently trying to figure out how to flash without having to use the SAM card. I downloaded the example from ST and am trying to run through the  B-U585I-IOT02A TFM exam...

JamesB_0-1740680927984.png
JamesB by Associate II
  • 2100 Views
  • 4 replies
  • 0 kudos

Resolved! STM32L562 - AES-CMAC functionality?

Hello community,I need to use the AES-CMAC functionality of the STM32L562QE.The datasheet says that it is supported :But it seems that the reference manual doesn't say anything about CMAC functionality.Is there really a way to use the AES coprocessor...

Adrian__0-1740650764416.png
Adrian_ by Associate
  • 1262 Views
  • 1 replies
  • 0 kudos

Resolved! Debug Authentication Failed

My H5 DK board is in TZ-CLOSED state (after --sfi-flash), I am unable to put it in "Level 1/2/3 Intrusive Debug" state no matter what combinations of keys and certificates to use (including key_1_root.pem and cert_root.b64). Only Full regression work...

Thatseasy by Associate III
  • 3943 Views
  • 2 replies
  • 0 kudos

Resolved! Is it coming official update of SBSFU to support CubeMX?

Hello everyone,Now I'm developing an user application compatible with SBSFU on STM32CubeIDE.SBSFU itself is pretty nice, but I feel the development architecture and environment are a little bit old, like not supporting CubeMX.Fortunatelly, I succeede...

YUTA1 by Associate II
  • 2202 Views
  • 4 replies
  • 3 kudos

STM32WLxx DFU Error

Hi,I ported the SBSFU project to the LoRaWAN_AT_Slave routine, and tested DFU normally and it worked fine, but when I used the wrong file to upgrade, such as readme.txt, the upgrade process ran for a while, and then stopped, showed " Fw header authen...

ethan2_0-1740128888124.png
ethan2 by Associate II
  • 1652 Views
  • 3 replies
  • 0 kudos

Resolved! STSAFE-A110 STSAFEA_COMMUNICATION_ERROR on all reads

Hi,I ported example projects from en.x-cube-safea1\project\NUCLEO-L476RG for MbedTLS cryptolib for use on my B-U585I-IOT02A Discovery Kit. The STSAFE-A110 is powered correctly and NRESET is pulled high. It never errors on writes to the device, but al...

Resolved! STM32U585 - can't get SBSFU-example to work

Hi, I'm trying to adapt the SBSFU-Cube repository example for the B-U585I-IOT02A (STM32CubeU5\Projects\B-U585I-IOT02A\Applications\SBSFU, repository V1.7.0) to a custom PCB with STM32U585CITx. Since I don't have access to UART1 I changed it in com.h ...

AAArdvark by Associate II
  • 1265 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.