STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PCROP area of STM32L471

Hello,I'm looking for some clarification over how the PCROP area can be used.  The user manual for STM32L471 states that code in this area can be executed but that data at flash in this area cannot be read.   Does this mean if I put a decryption algo...

Resolved! How to modify MCUBoot example to fit the project?

Hi ST team,I am using STM32U5G9 in my project. It would need simple firmware update feature and the image would be received by UART from a zigbee module.I have read UM2851 and AN5447 application notes and check the SBSFU example in STM32CubeU5 packag...

STM32H562 program the OBK file with trustzone disabled

We need to develop an offline programmer to program the STM32H562VIT. The product state need to be changed to Closed with an OBK file programmed. The OBK data only in HDPL1.We can't simply use the RSS to program the OBK like STM32Cubeprogrammer. We c...

Nluke.1 by Associate II
  • 647 Views
  • 2 replies
  • 0 kudos

Can I Create Logging Functionality Within the Secure App

STM32 H573 TrustZone Enabled question. I'm executing the STM32 H573 example for TrustZone Enabled (OEMiROT, Secure, and Non Secure Apps).  I know the OEMiROT and Non Secure App prints out and logs info, but I want to be able to do that in the Secure ...

cgj004 by Associate II
  • 789 Views
  • 4 replies
  • 2 kudos

STM32H755 Security settings

Hello, I have an STM32H755 nucleo board and I want to use the secure memory area features but I need to clarify my understanding of the reference manual "rm0399" and some follow up questions.My understanding is that:From my normal code (non-secure) i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.