2025-11-14 11:36 AM
STM32 H573 TrustZone Enabled question.
/**
* @brief Non-Secure Call-able (NSC) function that returns the pointer
* to the Non-Secure World's _write (UART) function.
*
* The __attribute__ flag ensures the compiler generates the security veneer.
*/
__attribute__((cmse_nonsecure_entry))
int32_t NS_putc_utility(int32_t ch)
{
char buffer[1] = {(char)ch};
// Call the actual low-level _write function.
// The security veneer is wrapped around this function entry.
return _write(1, buffer, 1);
}
2025-11-15 11:07 AM
@cgj004 While you're waiting for more useful replies... note that you can assign hardware components to the secure domain. For example, you can assign some UART and use it for "secure" logs. Define _putc or _write functions in the secure code to output to that UART.
Sharing more details about your requirements helps receiving useful answers.
2025-11-17 10:02 AM
I just want to be able for the Secure Application to print out info like the Bootloader and the Non Secure App does.The tutorial walks you through all the steps and at the end, you open up a putty terminal, press the reset button on the board, and it prints out info from the Bootloader and Non Secure levels:
[INF] TAMPER Activated
[INF] Flash operation: Op=0x0, Area=0x0, Address=0x0
[INF] Starting Bootloader OEMiROT
[INF] Swap type: none
[INF] Swap type: none
[INF] Swap type: none
[INF] Swap type: none
[INF] Starting validation of primary slot(s)
...
etc...
I just want to be able to put logging in the Secure level as well since I want to make some changes there and possibly debug before jumping to Non-Secure Init:
2025-12-03 2:09 PM
Hello @cgj004 ,
You can initialize UART in secure application and use leaving peripheral and associated GPIO non secure.
When non secure application will start, it will also initialize UART and will work.
Best regards
Jocelyn
2025-12-08 5:11 PM
Thanks, I may get around to trying this at some point. But since I got the the debugger to attach and I can step through, this print logging is not as necessary any more.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.