2025-08-26 2:58 AM - last edited on 2025-08-26 3:05 AM by Andrew Neil
Hello, I have an STM32H755 nucleo board and I want to use the secure memory area features but I need to clarify my understanding of the reference manual "rm0399" and some follow up questions.
My understanding is that:
Q1: If I don't call the RSS_exitSecureArea can I keep the secure code running on CM7, Can I run a normal non-secure application on CM4?
Q2: Does the RSS have a feature to authenticate a bootloader code and if the answer is yes, where is that documented?
2025-12-04 2:31 AM
Hello @immortal2113 ,
After creating the secure areas, it is not mandatory to call the exitSecureArea. Now, in such case, why creating this secure area if you don't use it ?
The RSS is not a secure boot. Reference Manual is a bit misleading on this point. There is no authentication done at this stage, just checking that your boot address is inside the secure area.
Best regards
Jocelyn
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.