STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-SBSFU: Can you update firmware using USART DFU?

All the provided examples are using USART YMODEM to transfer data. I know, that it really doesn't matter what kind of protocol you use as long as image is placed in a correct place in the memory, but I wonder if I can use DFU feature to update firmwa...

Hammad by Associate
  • 1419 Views
  • 1 replies
  • 0 kudos

Secure boot resources

HelloDo I unterstand correctly that the recommended secure boot option for STM32L4 is SBSFU?It seems that the only resource on how to get started with examples is the playlist on YouTube where a non signed exe from google drive has to be installed.Is...

MC.5 by Associate II
  • 484 Views
  • 1 replies
  • 0 kudos

Provisioning STM32H5 via UART and RSS

Hi everyone,Hi @Jocelyn RICARD, @D.Botelho @Jocelyn RICARDyou made this small bootloader example for testing H7 security features, e.g. RDP:https://community.st.com/ysqtg83639/attachments/ysqtg83639/mcu-security-forum/6051/1/STM32H753_SecureMem_Examp...

aco990_0-1762269799560.png
aco990 by Associate III
  • 538 Views
  • 1 replies
  • 0 kudos

STM32H7Sx - Passing volatile data to lower HDPL levels

On a secured STM32H7Sx device (in CLOSED or LOCKED product state), what is the recommended way of passing volatile data to lower HDPL levels?According to the reference manual, the SBS_RSSCMDR register can be used to pass volatile data from HDPL 1, 2 ...

Eliasvan by Associate III
  • 483 Views
  • 1 replies
  • 0 kudos

PCROP, End-user usage example

Hello,I have already read the AN4758 application note and I still have a few questions regarding PCROP.I have a project for end-users where the main application provides functions (API) that users can call to develop their own code. I was originally ...

B.Kaya by Associate III
  • 722 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.