2023-11-23 10:26 PM - edited 2023-11-24 1:58 AM
Hi guys:
I initialed the RTC of STM32F103C8T6 by cubeMx and enabled the RTC global interrupt.
void HAL_RTCEx_RTCEventCallback(RTC_HandleTypeDef *hrtc) /* second callback */
{
RTC_DateTypeDef rtcDate;
RTC_TimeTypeDef rtcTime;
HAL_RTC_GetTime(hrtc, &rtcTime, RTC_FORMAT_BIN);
HAL_RTC_GetDate(hrtc, &rtcDate, RTC_FORMAT_BIN);
LOG_DBG("[20%02d-%02d-%02d(%d) ", rtcDate.Year, rtcDate.Month, rtcDate.Date, rtcDate.WeekDay);
LOG_DBG("%02d:%02d:%02d] tick[%5d]\n", rtcTime.Hours, rtcTime.Minutes, rtcTime.Seconds, HAL_GetTick());
}
I got the following output:
[2023-17-24(6) 23:59:58] tick[ 4140]
[2023-17-24(6) 23:59:59] tick[ 5175]
[2023-17-24(6) 00:00:00] tick[ 6210]
[2023-17-24(6) 00:00:00] tick[ 7245]
[2023-17-24(6) 00:00:01] tick[ 8280]
[2023-17-24(6) 00:00:02] tick[ 9315]
It is clear that the time 00:00:00 is output twice, and we can see the ticks are different, and the data still keep 24, NOT change to 25.
So my questions are:
1. Why the time "00:00:00" output twice?
2. Why the date NOT be updated after 23:59:59?
Thanks.
2023-11-23 10:51 PM
Dear @Junde ,
Please have a look on the month also , 17 ? Should be in range 1-12.
Hope it helps you.
ST1-32
2023-11-23 11:05 PM
Thanks for your reminder. I do ignore it.:rolling_on_the_floor_laughing:
I checked the code, and the reason is the MX_RTC_Init() function initials the RTC by BCD format:
/* Coded in BCD format */
#define RTC_MONTH_NOVEMBER ((uint8_t)0x11)
2023-11-24 12:33 AM - edited 2023-11-24 12:38 AM
The repeated 00:00:00 is probably consequence of the bizarre way how Cube/HAL handles calendar in 'F1. And I don't know the answer to question 2, but wouldn't be surprised if it turns out to be related. Also, do you use a genuine STM32F1xx, or a counterfeit clone (usually on a BluePill)?
'F1's RTC does not have native calendar, it's a simple counter. The "library" tries to keep it below seconds-equivalent of 24h, and when it detects it being above 24h, it decrements 24h from it and increments the date.
I am not going to find out the exact mechanism how this goes wrong in your case. You can look yourself, Cube/HAL is open source.
The remedy is in not using Cube/HAL at all, maintaining an epoch time in the counters, using a proper procedure to read them (see RM), and using standard C <time.h> facilities to calculate between epoch and calendar formats (with the Y2k38 caveat).
JW
2023-11-24 2:08 AM - edited 2023-11-24 2:29 AM
@waclawek.jan Thanks for your help.
Thanks for @STOne-32 's reminder, after I change the date format from Binary to BCD, the date can be updated normally.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.