STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! BLE on WB15CC (MB1641) limits notifications to 20 bytes

Dear friends, good evening.I am facing the following problem with my application using BLE with the MB1641 (STM32WB15CC):We had an app that worked with a device using another microcontroller (Nordic). We are adapting this device to an STM32 platform....

WhatsApp Image 2023-11-22 at 11.42.50.jpeg WhatsApp Image 2023-11-22 at 08.45.04.jpeg
Wiliam by Associate II
  • 3566 Views
  • 3 replies
  • 3 kudos

ADC reading error

I am using stm32f334r8 for digital power control. I have configured ADC using cube mx Lower level. ADC reads 0 for 40mv input even though ADC is configured to 12bit and 181  sampling cycles. I also tried calibrating ADC before conversion is started. ...

vasudev by Associate II
  • 1827 Views
  • 2 replies
  • 0 kudos

My microcontroller getting shorted while powering up.

While powering up all of my Microcontrollers were getting shorted, checked the voltages of all the capacitors and the MCU has a dedicated power line . And checked the ripple and initial power up data,everything is fine only. But still the MCU getting...

Bosss by Associate II
  • 6503 Views
  • 7 replies
  • 0 kudos

USBPD with STM32G0B1 doesn´t work

Hi, I´m trying to get a STM32G0B1 running with USBPD and a higher PDO voltage (20V). Therefore I followed the instructions in chapter 9 of STM32StepByStep:Getting started with USB-Power Delivery Sink - stm32mcuUnfortunately the user_services don´t co...

AWack by Senior
  • 1312 Views
  • 1 replies
  • 0 kudos

Resolved! DMA on STM32G473 always generates transfer error

Hi, Iam using a STM32G473 controller and want to do the following:I want to output an analog curve, stored in a RAM buffer.Timer6 is the timebase for transfering the the data from RAM buffer to DAC via DMA.So I selected the DAC as trigger source for ...

Moritz1 by Associate III
  • 3486 Views
  • 5 replies
  • 1 kudos

Looking for Libraries

Hello, i'm looking for stm32 libraries for the board STM32G071RB.In particular i'm trying to da many schetch using the device that i'm used before with Arduino Ide with the board ARDUINOUNO or ARDUINONANO .Devices LCD i2c , module HC05 for IOT gas se...

Paul2014 by Associate
  • 1555 Views
  • 1 replies
  • 0 kudos

Why RTC always count twice 00:00:00?

Hi guys:I initialed the RTC of STM32F103C8T6 by cubeMx and enabled the RTC global interrupt.  void HAL_RTCEx_RTCEventCallback(RTC_HandleTypeDef *hrtc) /* second callback */ { RTC_DateTypeDef rtcDate; RTC_TimeTypeDef rtcTime; HAL_RTC_Ge...

Junde by Senior III
  • 2868 Views
  • 4 replies
  • 6 kudos

Resolved! Recommended course of action for Unused pin of STM32 MCU

Dear ST Community membersI am currently designing a PCB and utilizing the STM32G473VET6 MCU. I have noticed that there are several unused pins. Should I leave these pins unconnected or is there a recommended course of action for dealing with them?tha...

Neeraj by Associate II
  • 24117 Views
  • 15 replies
  • 7 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.