2017-03-09 6:50 AM
Hi all:
The document says the power consumption is 112 uA / MHz.
But the power supply has offered 56mA current.
I measure the IDD pin, the result is only 16 mA.
Is the consumption due to ST-Link part ?
If yes, could I cut off the ST-Link part?
Thank you in advance.
2017-03-09 7:07 AM
The datasheet contains multiple power consumption scenario. Find the entry which is closest to your situation (supply, MHz, peripheral on or off, etc..) What is on a datasheet is guaranteed and more specific. (let's say second order of precision). I haven't looked at the schematic to understand where the current is going after the jumper... check it out.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.