2017-03-08 6:04 AM
Hi,
Followed a similar thread with SPI Rx Slave in
https://community.st.com/0D50X00009XkhZKSAZ
followed the same, but used Channel 3 instead..
The RM0364, DocID025177 Rev 2, Page &sharp179, Figure 20. STM32F334xx DMA1 request mapping,
states that DMA1 Channel 3 needs remapping to be used with SPI1. It appears to be the same for
any DMA Channel.
Nevertheless it appears that all SPI TX DMA transfers do need a DMA remap, according to the
figure 20. But well, that aside ..
Though I tried remap, there appears to be no change. I have connected a scope to the SCK pin,
there appears to be no activity at all.
Any thoughts, on the following code ?
Thanks.
null2017-03-08 9:51 PM
Replying to my own post,
Found a small bug, which caused no activity on the SCK line:
It should've been Tx instead of Rx:
/* DMA request enable */
SPI_I2S_DMACmd(SPI1, SPI_I2S_DMAReq_Tx, ENABLE);I now see one single SCK pulse and the following debug output:
========================
SPI1 LCD DMA Debug
========================
Frames init
SPI1 Init
DMA1 CH3 Init
NVIC Init
CH3 IRQ
TE3
IRQ enabled
Backlight ON
-------------= SPI1 REG dump =-------------
SPI_CR1 : 0xc36d
SPI_CR2 : 0x702
SPI_SR : 0x02
SPI_DR : 0x00
SPI_CRCPR : 0x07
SPI_RXCRCR : 0x00
SPI_TXCRCR : 0x00
-------------------------------------------
Since the original issue past, Wondering now why the TE3 ?
Any thoughts/suggestions/comments ?
Thanks.
2017-03-09 12:57 AM
If there is no example in Cube for this and assuming this is SPI master mode, try first in 2 lane mode with TX and RX connected to a DMA stream. The RX stream, if unused, can cycle through a few RAM bytes, and the GPIO does not need to physically exist.
While in std lib, this code seems quite explicit on how to play with SPI as master and DMA (SPI IP without FIFOs)
2017-03-09 9:05 AM
Thanks. I will take a look. There weren't any examples for the F334 and hence..
Moving:
SPI_Cmd(SPI1, ENABLE);
immediately after SPI_Init()
fixed the issue. Weird though..
SPI_Init(SPI1, &spi);
SPI_Cmd(SPI1, ENABLE); putstr(USART1, 'SPI1 Init\r');We’re moving the ST Community to a new platform to give you a better and more reliable community experience.