2018-02-25 12:55 PM
Hi
i do have the B-L072Z-LRWAN1 board and try to make a End-node..
When i want to debug the Stm-cube LRWAN END NODE exsample it gives me a failure ...the port is in use ?
What can i do wrong ...Normally absolut no problems...
Both Keil and openstm32 make the failure..
Anyone know ?
Hjalmar
Solved! Go to Solution.
2018-02-26 12:23 PM
Hello
Skovholm_Hansen.Hjal
,to achieve lowest possible current consumption, SWD pins are set to analog mode without pull resistors and this is causing you error on debug.
Check for define LOW_POWER_DISABLE and uncomment it. In this case, pins won't be changed and you should be able to debug.
Best regards,
Tilen
2018-02-25 1:16 PM
Disable low power modes where it turns OFF the JTAG/SWD interface.
See define LOW_POWER_DISABLE
2018-02-25 3:51 PM
it gives me a failure ...the port is in use ?
Please post the exact message you get, and describe the exact steps you take up to getting it.
2018-02-26 12:23 PM
Hello
Skovholm_Hansen.Hjal
,to achieve lowest possible current consumption, SWD pins are set to analog mode without pull resistors and this is causing you error on debug.
Check for define LOW_POWER_DISABLE and uncomment it. In this case, pins won't be changed and you should be able to debug.
Best regards,
Tilen
2018-02-26 1:34 PM
Hi tilen
thanks for your help.
it worked...
i do program on the board you teach us in Copenhagen, and my lora node is doing progress.
i did also set up my own lora gateway on a raspberry so Now looking into a very interesting World.
just order some stm32L0 sx1276 and Will get Them to work When finish with the initial test on this board...
thanks for you help again
hjalmar
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.