STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Evaluation board STM32L073VZ - DFU Update

Posted on February 16, 2018 at 07:25Hello, i am working with the STM32L073x on the evaluation board STM32L073VZ and the Nucleo-L073RZ and I want to figure out the functionality of the USB DFU Update via internal bootloader. As descibed in several ap...

klaus23 by Associate
  • 1956 Views
  • 4 replies
  • 0 kudos

Pin consumption

Posted on February 26, 2018 at 14:39Hi all,I have a STM32L073 on a custom application. I'm having some strange behavior with open pins. Particularly, PH1 and PC3 are floating, nothing is connected to them. When both are set as Digital In the current...

Resolved! Nucleo64 Power Measurement

Posted on February 26, 2018 at 17:34I'm measuring the current on JP6 (IDD) and I see 4mA at the lowest when running the Power_Management sample or even holding the MCU in reset. I am powering the board via the USB connector. Is this incorrect?I've t...

Konami by Senior II
  • 4030 Views
  • 14 replies
  • 0 kudos

FatFs f_open() fails after upgrading to STM32F4 FW pkg 1.17

Posted on November 03, 2017 at 19:53 I have two versions of my project exported from the CubeMX, one for the MDK-ARM and the other for the gcc-based Eclipse IDE (AC6). Both projects built with STM32F4 firmware package 1.1. After upgrading the fir...

Zaher by Senior II
  • 13330 Views
  • 29 replies
  • 0 kudos

STM32F072C8T6 USB-C : X-CUBE-USB-PD

Posted on February 26, 2018 at 17:37HelloI would like to use an STM32F072C8 instead of STM32F072RB with ST example : MB1303ConsumerRTOS.To ease the task, I would like to know, if it was possible to have the Cube configuration of the design. The STM3...

Configuring CAN - error with CubeMX 4.24 STM32F4 1.19.0 ?

Posted on February 26, 2018 at 17:15I try to configure a CAN peripheral in the same kind as before. I want to use the new CAN driver functions.As soon as I’am setting the clock to HSE and 168 MHz no change in CAN is possible. Setting Clock to HSI se...

fe3 by Associate III
  • 766 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.