2019-01-02 3:33 AM
hi,
we are trying to measure vrefint using adc of stm32l1xx. the converted data is keep on varying between 0 to 3000 (decimal). we are not sure where is the problem. can anyone help on this issue? here is the sample code:
//hsi clock is enabled in startup
ADC_BankSelection(ADC1, ADC_Bank_A);
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = DISABLE;
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T9_CC2;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = 1;
ADC_Init(ADC1, &ADC_InitStructure);
ADC->CCR |= 1 << 23; //enable vrefint
ADC_RegularChannelConfig(ADC1, ADC_Channel_17, 1, ADC_SampleTime_4Cycles);
ADC_Cmd(ADC1, ENABLE);
/* Wait until the ADC1 is ready */
while(ADC_GetFlagStatus(ADC1, ADC_FLAG_ADONS) == RESET)
{
}
ADC_SoftwareStartConv(ADC1);
while (1)
{
if(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC))
{
ADC_ConvertedValue = ADC_GetConversionValue(ADC1);
printf("\r\n data = %d ", ADC_ConvertedValue);
for(i=0;i<800000;i++);
ADC_SoftwareStartConv(ADC1);
}
}
tried with different system clock (msi, hsi, hse). but still converted data is keep on changing.
thanks ,
elavarasan s
2019-01-02 3:39 AM
Look in the datasheet and reference manual. ADC_SampleTime_4Cycles seems very short.
2019-01-02 3:55 AM
Check if there is a power enable control bit for Vref block. (ref man)
2019-01-02 10:49 PM
i tried with all sample rates. but result is same. we have checked one more analog input (2.5v) is connected with PC5. getting the same result. getting random data after conversion. strange. we are missing something???
2019-01-02 10:54 PM
there is no power enable for vref. but VREFINTRDYF is set in PWR_CSR register. we have checked one more analog input (2.5v) is connected with PC5. getting the same result. getting random data after conversion. strange. are we missing something???
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.