STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO H743ZI ETHERNET COMMUNICATION PROBLEM

Posted on December 11, 2017 at 14:04I have a NUCLEO H743ZI board and I want to communicate pc and nucleo-board by using LAN8742 on NUCLEO-H743ZI. I tried many of times but I havent succeeded this. I made communication between pc and STM746VGT6 micro...

Duygu A by Associate
  • 1287 Views
  • 2 replies
  • 0 kudos

ADC low power

HAL_ADC_DeInit()enter stop modeclock configHAL_ADC_Init()is it a good method to do low power?

stm32l1xx adc is giving random data after conversion done

hi,we are trying to measure vrefint using adc of stm32l1xx. the converted data is keep on varying between 0 to 3000 (decimal). we are not sure where is the problem. can anyone help on this issue? here is the sample code: //hsi clock is enabled in st...

es.18 by Associate II
  • 2423 Views
  • 4 replies
  • 0 kudos

Resolved! Where is pin Nr 1?

Hello,On this picture, which is the pin Nr 1?Top right or bottom left ?ThanksJulien

JulienD by Senior
  • 2434 Views
  • 4 replies
  • 0 kudos

Resolved! How can we use RS-485 in full-duplex ?

Hello,We need to use RS-485 in full duplex, and with the flow control (DE).Is it that when we configure DE with RS485 is shall be used as half duplex ?can I configure rs232 pins with RTS (instead of DE) before converting voltage to rs-485 levels ?Wil...

ranran by Senior II
  • 10661 Views
  • 16 replies
  • 0 kudos

Resolved! STM32H7 SPI ISSUE

Posted on April 06, 2018 at 16:43 Hai, Iam using the STM32H743VIT controller , We are using the spi4 in our board ,we generated the code using the cube mx nothing is coming(CLK and SIN)when transmit the data using the function ( HAL_SPI_Transmit(SP...

MANISH by Associate II
  • 5375 Views
  • 10 replies
  • 0 kudos

internal temperature sensor stability

Hi guys and girls!I'm using STSPIN32F0, an MCU with built-in 3-phase motor driver and I'm trying to read internal temperature sensor. What I'm getting back looks to me like random walk within range of about 10 degrees Celsius (please see attachment)....

Misha K by Associate III
  • 2524 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.