2019-01-02 3:30 AM
Hello,
On this picture, which is the pin Nr 1?
Top right or bottom left ?
Thanks
Julien
Solved! Go to Solution.
2019-01-02 6:08 AM
Bottom Left (see Nucleo-144 Board), the top-right is the ejector mark from the mold.
2019-01-02 3:41 AM
Look in the datasheet under Device marking. Normmally when the labels are readable like normal text, Pin 1 is bottom left
2019-01-02 6:08 AM
Bottom Left (see Nucleo-144 Board), the top-right is the ejector mark from the mold.
2019-01-02 6:26 AM
Ok, I always thought that labels were not a reliable way to identify pins.
Btw, in CubeMX, it is a third orientation...
I just need to unsoldier it.... :(
Thanks.
2019-01-02 9:38 AM
There have been previous threads where I've posted pictures. Different manufacturing sites have different equipment so there are usually a couple of variations in the plastic and printing or laser marking.
I think the marking could be a lot move obvious and consistent.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.