2025-08-26 6:05 PM - last edited on 2025-08-26 10:44 PM by Imen.D
Target MCU: STM32L151ZETx (LQFP144)
Main Clock Frequency: 32 MHz
When the MCU is first powered on, it takes about 41 ms to reach the while(1) loop in the main() function, based on the code shown below.
For my product requirements, I would like this startup time (from power-on to reaching while(1)) to be reduced to around 16 ms.
Is there any way to achieve this reduction? Any suggestions or optimization techniques would be greatly appreciated.
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "adc.h"
#include "dma.h"
#include "rtc.h"
#include "tim.h"
#include "usart.h"
#include "gpio.h"
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
int main(void)
{
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_ADC_Init();
MX_TIM5_Init();
MX_TIM2_Init();
MX_TIM3_Init();
MX_TIM4_Init();
MX_TIM6_Init();
MX_RTC_Init();
MX_USART1_UART_Init();
MX_USART3_UART_Init();
/* Start timers */
HAL_TIM_Base_Start_IT(&htim2); // TIMER2(100us)
HAL_TIM_Base_Start_IT(&htim5); // TIMER5(1ms)
HAL_TIM_Base_Start_IT(&htim3); // TIMER3(10ms)
HAL_TIM_Base_Start_IT(&htim4); // TIMER4(20ms)
HAL_TIM_Base_Start_IT(&htim6); // TIMER6(1440Hz)
HAL_TIM_PWM_Start(&htim5, TIM_CHANNEL_1);
/* Infinite loop */
while (1)
{
}
Edited to apply source code formatting as recommended in this guideline How to insert source code.
2025-08-26 7:07 PM
Toggle pins at various points during startup to see where the most time can be saved. Toggle immediately after Reset_Handler to see the minimum time.
A few things in particular will have large effects:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.