STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC Fluctuation or Oscilation

HelloI am using NUCLEO-G474RE board to sample voltages from the the Battery management board. In the PCB board, I have opamp voltage divider to step down voltages around 24Volts to 2.5V level to be read from the STM. Please refer to the voltage divid...

ytshin0877_1-1756187340360.png IMG_3053.jpeg IMG_3055.jpeg IMG_3054.jpeg

Resolved! STM32L053 LSE CSS not trigger

I tested the LSE CSS function on the Nucleo-L053, but I found that short-circuiting the crystal oscillator pins failed to trigger the CSS interrupt. The code configuration is as follows plz give a clue or the flow of LSECSSvoid SystemClock_Config(voi...

ShimiaoWang_0-1755742211333.png

Resolved! FDCAN H5 Memory Access Failure

I'm experiencing FDCAN Memory Access Failures on the STM32H503KBUX during CAN Rx. I am also experiencing intermittent CAN Rx message drops (every 1 in a 200), and I believe the two are related since no others errors are firing. I know the drops are h...

dnugent_0-1755890008288.png
dnugent by Associate II
  • 1186 Views
  • 5 replies
  • 0 kudos

STM32F207ZGT6 revision

Hello,Is it possible that STM32f207ZGT6 purchased in 2025 from an official distributor have an old silicon revisionrev_id = 0x200f? 

stmf207.jpg
pioczl by Associate
  • 681 Views
  • 2 replies
  • 0 kudos

Resolved! SPI Always Reads 0

I am having a problem reading SPI data on an STM32F407 where it always returns 0x00. I actually have this working using HAL on the same hardware, however for legacy reasons I need to get this working with SPL. This application is just sending clock s...

twjudge by Associate
  • 888 Views
  • 1 replies
  • 1 kudos

Resolved! PCB design with stm32h7 series (144 pin)

According to some reference it is good to have ground polygon under IC 1. Is it okay to have ground polygon under IC? 2. Does it effects heating issue?3. I saw two hole behind the IC of nucleo 144 board. What that mean? 

Ironman by Associate II
  • 1662 Views
  • 6 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.