2013-05-14 2:40 PM
I am trying to use GPIO Pin PE9 and PE10 as outputs to a system. From using the STM32L1Discovery Board I know that the GPIO Output voltage should be 3 V. But when I am using the F4 BOard my output on PE9 is 2 V and PE10 is 1 V. When I make the pins low, I am reading 7 mV so I know that the pins are turning on, but does anyone know why I am only getting a 2V output?
2013-05-14 6:58 PM
The pins don't have any other utilization on the board.
Consider how you have them configured. Consider how they are loaded externally.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.