STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C Clock Control - Fast Mode

Posted on April 17, 2013 at 12:12Section 2.6.8 of RM0038 states:''fPCLK1 must be a multiple of 10MHz to reach the 400kHz maximum I2C fast clock mode''how can I calculate the maximum I2C frequency I can achieve using a 4.2MHz fPCLK1this information d...

Exprienced but new to STM32 with questions

Posted on May 14, 2013 at 04:41Ti has dropped its M3 Stellaris line. Their new M4 does not have I2S or extended memory controllers. It takes time to know a product line, which parts are up and coming, which ones to avoid, and which tool set. I'm sta...

how to read protect F4 with Eclipse + openOCD

Posted on April 29, 2013 at 20:22hello forum , I am using openOCD   JTAG  with Eclipse for downloading my code into STM32F4 I have a question ; how to read protect my F4 after I download my code ? thank you #eclipse-openocd-read-protect

stm32f103 adc connected to potentiometer

Posted on May 10, 2013 at 09:00i have connected a potentiometer(via stm32f103 3.3 v) to stm32f103 adc channel 1 (ADC1_IN1), with continuous mode, sampling 1.5. i am getting the values in DR register, and want to change the values during run time by ...

aman by Associate II
  • 4440 Views
  • 9 replies
  • 0 kudos

SPI Problem(NO SCK Signal when receiving)

Posted on May 15, 2013 at 05:08Hi, everyone. I am trying to control a slave device by SPI Communication. But I have a problem with SPI, SCK is not output when receiving a data. Tx is OK. Why does this problem happen? I hope you help me to slove this...

andykim by Associate II
  • 1175 Views
  • 2 replies
  • 0 kudos

STM32F4Discovery GPIO

Posted on May 14, 2013 at 23:40I am trying to use GPIO Pin PE9 and PE10 as outputs to a system.  From using the STM32L1Discovery Board I know that the GPIO Output voltage should be 3 V.  But when I am using the F4 BOard my output on PE9 is 2 V and P...

STM32L discovery I can not load program from Keil

Posted on May 14, 2013 at 17:31I have 3 STM32L152 discovery which anser ''Unknown target connected'' when I load a program from keil.I try  setting BOOT0 HIGH when I push the  reset Button .There no result.Best regardsYves de Brest

yves2399 by Associate II
  • 1016 Views
  • 1 replies
  • 0 kudos

Playback PCM audio file

Posted on May 13, 2013 at 11:19Hi, I am trying to playback a file with short PCM data recorded at 8KHz, 16bits, mono. I have tryed to configure the I2S with ''I2S_Standard_PCMShort'' but I can�t hear any sound. I have made a file like the file ''aud...

rafael23 by Associate II
  • 3361 Views
  • 5 replies
  • 0 kudos

USART interrupt problem

Posted on May 13, 2013 at 11:10Hi guys, i've a problem with USART communication using interrupts.Using only USART device, the communication works correctly.When i try to using the usart device with some other timers interrupt routines with timers ab...

pietro2 by Associate II
  • 1842 Views
  • 3 replies
  • 0 kudos

Why is the IrDA Baudrate limited to 115.2kBd?

Posted on May 13, 2013 at 20:56Hi, in STM32F4 RM 26.3.12 it says, that ''USART supports only bit rates up to 115.2kBps for the SIR ENDEC''. Can anyone tell me the reason? (115.2kBd must be an increibly low data rate for a 168MHz processor). In fact ...

flyer31 by Senior
  • 2031 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.