cancel
Showing results for 
Search instead for 
Did you mean: 

Export pinout

mksws
Associate

I've just installed CubeMX2 to start work on a new project using STM32C552xxx.

My normal practice is to export a .csv of all the processor pins along with the alternate functions and in CubeMX this is easy.

But Cube MX2 only exports a .csv like this:

PositionPinTypeSignalsPin labels
1PE2gpio  
2PC13gpio  
3PC14-OSC32_IN(OSC32_IN)gpio  

Please tell me there is an option to list all the alternate functions in the.csv.

It is quite impossible to to allocate the pins and peripherals for a new design working only with the pop_up detail view in CubeMX2. 

An acceptable alternative would be for ST to just publish such a .csv some where.

MK

3 REPLIES 3
Andrew Neil
Super User

@mksws wrote:

Please tell me there is an option to list all the alternate functions in the.csv.


+1 to that!

There was a lot of discussion about getting that from CubeMX - I very much hope it hasn't been lost in MX2 ...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Oussama_TROUDI
ST Employee

Hello @mksws,
Thanks for your feedback and welcome to ST Community.

The team is already working on it internally, and an internal ticket has been created to track this request to export pinout with alternate functions. I will keep you posted with any updates.

Internal ticket number: CDM0057819 (This is an internal tracking number and is not accessible or usable by customers).

Regards,
Oussama


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Thank you for the update.