2013-05-14 8:08 PM
Hi, everyone.
I am trying to control a slave device by SPI Communication. But I have a problem with SPI, SCK is not output when receiving a data. Tx is OK. Why does this problem happen? I hope you help me to slove this problem. The belowing is my codevoid bsp_init_rcc(void)
{ /* SYSCLK, HCLK, PCLK2 and PCLK1 configuration -----------------------------*/ /* RCC system reset(for debug purpose) */ RCC_DeInit(); /* Enable HSE */ RCC_HSEConfig(RCC_HSE_ON); /* Wait till HSE is ready */ HSEStartUpStatus = RCC_WaitForHSEStartUp(); .................................................. /* Enable GPIOA, GPIOB, GPIOC, GPIOD, GPIOE and AFIO clocks */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB |RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOD | RCC_APB2Periph_GPIOE | RCC_APB2Periph_AFIO, ENABLE); /* Enable peripheral clocks --------------------------------------------------*/ /* SPI1 clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE); /* SPI2 Periph clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE); }void bsp_init_gpio(void)
{ GPIO_InitTypeDef GPIO_InitStructure; /* Configure SPI1 pins: SCK, MISO and MOSI ---------------------------------*/ /* Confugure NSS, SCK and MOSI pins as Alternate Function Push Pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_7; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Confugure MISO pin as Input Floating */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure);/* Confugure NSS pin as Output */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 ; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); }void spi_init(void)
{ /* SPI1 configuration ------------------------------------------------------*/ SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Hard; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_4; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI1, &SPI_InitStructure); /* Enable SPI1 CRC calculation */ SPI_CalculateCRC(SPI1, ENABLE);SPI_SSOutputCmd(SPI1, ENABLE);
/* Enable SPI1 */
SPI_Cmd(SPI1, ENABLE); SPI_NSS_High(); }void SPI_tx_data(uint8_t data)
{ /* Wait for SPI1 Tx buffer empty */ while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);SPI_NSS_Low();
SPI_I2S_SendData(SPI1, data); while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_BSY) == SET) ; SPI_NSS_High(); }uint8_t SPI_rx_data(void)
{ uint8_t data;/* Wait for SPI1 data reception */
while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET); SPI_NSS_Low(); data = SPI_I2S_ReceiveData(SPI1); SPI_NSS_High(); return data; } Please help me2013-05-14 9:21 PM
Why does this problem happen?
Because the bus is symmetrical, as a Master device it clocks out on one edge, and back on the other. ReceiveData just reads a holding register, it does not clock. You'll need to send a junk/dummy byte to generate the clocks to load the receive register.2013-05-14 10:11 PM
Hi clive1
Do you mean the folllowing coding?uint8_t SPI_rx_data(void)
{ uint8_t data; SPI_NSS_Low(); SPI_I2S_SendData(SPI1, 0x00); while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_BSY) == SET) ; SPI_NSS_High(); /* Wait for SPI1 data reception */ while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET);data = SPI_I2S_ReceiveData(SPI1);
return data; } By a dummy byte tx, I can see a data output from the slave device. But I cann't read the recevied data at the data register of the STM32F103, which is received from the slave. How can I do this? Thanks clive1.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.