2013-05-14 8:31 AM
I have 3 STM32L152 discovery which anser ''Unknown target connected'' when I load a program from keil.
I try setting BOOT0 HIGH when I push the reset Button .
There no result.
Best regards
Yves de Brest
2013-05-14 9:11 AM
Make sure you've configured the Debugger to use SWD mode.
Ensure you have current drivers and firmware. Confirm connectivity/function with the ST-Link Utilities. The older firmware will expect you to use the ''ST-Link (Deprecated Version)'' connection in Keil. The newer firmware ''ST-Link Debugger'' There have classically be download issue with Keil/ST-Link (Flash->Download), but the debug/download option should work.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.