2024-11-15 8:25 AM - last edited on 2024-11-18 3:19 AM by mƎALLEm
I get the time in one thread with following code:
RTC_TimeTypeDef ti = {0};
RTC_DateTypeDef da = {0};
HAL_RTC_GetTime(& hrtc, ti, RTC_FORMAT_BIN);
HAL_RTC_GetDate(& hrtc, da, RTC_FORMAT_BIN);It jumps from 12:59 to 1:00 instead 13:00,
With another project which uses an older firmware and different pcb but same MCU this does not happen.
Can this be a probem in the Cube Ide HAL 1.28.1?
Or a problem with the RTC itself? I have only one prototype yet, but I will check next week with other prototypes.
HAL_RTC_GetTime contains the following code:
sTime->Hours jumps from 13 to 1 but sTime->TimeFormat remains 0.
I use 24 hours, but even if the settings would be 12 hours, the sTime->TimeFormat should be set after going from a.m. to p.m.
sTime->Hours = (uint8_t)((tmpreg & (RTC_TR_HT | RTC_TR_HU)) >> RTC_TR_HU_Pos);
sTime->Minutes = (uint8_t)((tmpreg & (RTC_TR_MNT | RTC_TR_MNU)) >> RTC_TR_MNU_Pos);
sTime->Seconds = (uint8_t)( tmpreg & (RTC_TR_ST | RTC_TR_SU));
sTime->TimeFormat = (uint8_t)((tmpreg & (RTC_TR_PM)) >> RTC_TR_PM_Pos);
The jump happens also if I set the time to 12:59 and afterwards put the MCU some minutes into power saving mode. I am not sure if the jump happens in the RTC (but worked previously) or after initialising and restoring the RTC backup.
Solved! Go to Solution.
2024-11-19 8:27 AM
In the meantime I have power cycled the device and the problem disappeared.
An there was also an uninitialised variable once there:
RTC_TimeTypeDef ti = {0};
RTC_DateTypeDef da = {0};
HAL_RTC_GetTime(& hrtc, ti, RTC_FORMAT_BIN);
HAL_RTC_GetDate(& hrtc, da, RTC_FORMAT_BIN);ti and ta had not been initialised, but this should not have an influence on the internal RTC storage.
I wonder why the setting is not corrected on startup (w/o power cycle).
rtc handle hrtc is a global variable which is initialised to 0:
RTC_HandleTypeDef hrtc;
MX_RTC_Init sets:
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
it calls:
HAL_RTC_Init
In that function there is:
/* Check whether the calendar needs to be initialized */
if (__HAL_RTC_IS_CALENDAR_INITIALIZED(hrtc) == 0U)
Within this if, the CR would be set:
hrtc->Instance->CR |= (uint32_t)(hrtc->Init.HourFormat | hrtc->Init.OutPut | hrtc->Init.OutPutPolarity);
The problem was, that the hour formate was not set because __HAL_RTC_IS_CALENDAR_INITIALIZED delivered true.
Why the odd value of the CR came into it, don't know.
2024-11-19 8:40 AM
You correctly don't change the RTC settings once set up and running, but if incorrect bits in CR get set, they remain set until the next backup-domain reset (battery removal, or explicit backup-domain reset for whatever reason).
> Why the odd value of the CR came into it, don't know.
It's usually consequence of uninitialized struct in calling HAL_RTC_SetTime() where the DayLightSaving and StoreOperation fields are OR-ed to RTC_CR.
As I've said in the pointed-to article, it may be also consequence of the backup-domain brownout, if that's a possibility in your hardware setup.
JW
2024-11-20 3:03 AM
Calling HAL_RTC_SetTime() used a local RTC_TimeTypeDef, which was uninitialised.
2024-11-21 4:42 AM
Thanks for coming back with this information.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.